7/16/2007 11:16 PM | |
Posts: 4 Rating:
|
Hello all, Thank you J_Bell for your earlier help. I am not trying to emulate a PNIO device working with CPU 312C with CP 343-1 (Please see attachment) The purpose is: - Send data block to the device - Recieve data block from device For emulation I have 2x CPU312C and 2x CP343-1. I would prefer to use PNIO commands for tis purpose. I observed that I could not connect second CP 343-1 with Profinet Ethernet when I declare first one as PNIO Controller. To solve this, can someone suggest me the best way? I tried many many possible solutions (please see attachment) like I added one more CPU and CP in present project with one CPU and CP and tried with ISO-on_TCP (although not preffered) but I do not know how can I write SEND/RCV program or download fresh configuration in in newly added CPU? Please note that I am using a normal Ethernet LAN Cable (not crossover) as automatic crossover detection is added feature to CP (suggested in Siemens manual) AttachmentCPU_CP_emulationTest.pdf (725 Downloads) |
7/17/2007 5:16 PM | |
Posts: 4 Rating:
|
Dear Bell There are many in this forum who listen to you I did at my best what you adviced me and the present condition is better but not good to start programming: - both CPUs are in RUN mode - CP_controller: SF on, BF blinks, RUN on, RX/TX blinks and P1(port I am using)is on (yellow) - CP_device: SF OFF, rest every LED has same statu as of controller I dont knowbut would it be possiblefor you to please have a look at HW config of my program and tell me what I am doing wrong. Regarda Ronny AttachmentPNIO_tes.zip (560 Downloads) |
7/18/2007 9:35 AM | |
Posts: 5822 Rating:
|
Dear Ronny, try this Project, I guess it should work. Best regards J_Bell AttachmentPNIO_tes2.zip (716 Downloads) |
Follow us on