2/14/2015 10:04 AM | |
Posts: 1 Rating:
|
Hi everybody, Firstly the configuration is seen in the pdf file. My cpu 313C-2DP connects a IM 151-1 basic(ET200s) module via profibus. And a 4AI-TC-ST (134-4jd00-0ab0) module connects the IM151-1 module. I prepared and loaded the configuration. But I can't receive any analog value of chanels of 4AI TC ST module. If ı select the any s7-1200 cpu and connect the IM151-1 module via profibus, ı can see value of analog input channels in the watch table. However ı wrote a simple network in main(OB1) for moving the value of analog channel 1. but ı cant download the main program. Have anybody ever seen this problem? Can anyone help me? Best regards. Attachmentimage.pdf (74 Downloads) |
2/14/2015 10:08 AM | |
Posts: 8946 Rating:
|
First, use a flagword < 128 inside CPU313! |
Follow us on