Industry Online Support
Technical Forum
4/25/2011 6:17 PM | |
Posts: 20 Rating:
|
Dear Friends Can I use CPU 314C-2DP as SLAVE ? SIEMENS Order is : 6ES7314-6CG03-0AB0 |
4/25/2011 7:19 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating:
|
Hello Marcopolo; The integrated DP interface of all -2DP or -2PN/DP CPUs can be setup as Profibus master or profibus slave. Look at the following configuration examples; you can use replace the example PLCs by your ownexact modelwhen you configure your project: S7 as slave, master is in the same Step 7 project: DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3 Slave and master are in different projects: Master-slave connection between two CPUs in different projects Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/25/2011 7:19 PM |
|
5/3/2011 5:21 AM | |
Posts: 20 Rating:
|
Dear DANIEL I have have attached some screens that I hope be useful,Thanks for your pursuiting. I'll be remain. Attachmentdp fault.zip (87 Downloads) |
5/3/2011 7:16 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, What about the hardware connection there? Did you check the cable and connectors? Best regards, Hristo Mihalev |
5/3/2011 7:42 AM | |
Posts: 20 Rating:
|
Dear UMENCHO Connections are ok,and everything tested |
Last edited by: Marcopolo at: 5/3/2011 7:43 AM |
|
Follow us on