1/22/2013 10:36 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, You can use MPI or Profibus to connect to this panel. A memorycard is not needed to use this panel. Memory card can be used for transfering recipes and for backup. Further information in:SIMATIC HMI HMI Device TP 177A, TP 177B, OP 177B (WinCC flexible) Regards, Marcjan |
Last edited by: Marcjan at: 1/22/2013 10:46 AMProblem solved? |
|
1/22/2013 10:37 PM | |
Posts: 33 Rating: (0) |
thanks marcjan.. |
1/22/2013 10:37 PM | |
Posts: 33 Rating: (0) |
thanks Ste39.. |
1/24/2013 8:17 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello cy429, Here is Following Link of FAQ Which Will solved all the Problem. How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? How do you use WinCC flexible to transfer a project to an operator panel via S7 routing? What transfer options are available in the various operator panels? |
Ammy |
|
1/25/2013 12:16 AM | |
Posts: 33 Rating: (0) |
Thanks Ammy |
Follow us on