11/4/2016 12:30 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, One way is this: How do you configure a connection between WinCC flexible Runtime ... there are other way also, depend what you want to do, if you want to own program on the PC side I had done long ago with Softnet software and CP and S7 300 via Profibus |
Last edited by: Ste39 at: 11/4/2016 12:34:14 PM |
|
11/9/2016 12:45 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
Hm, ho long is the distance from the Control Room to the machine? Christoph |
11/9/2016 1:01 PM | |
Joined: 10/22/2011 Last visit: 8/26/2024 Posts: 299 Rating: (1) |
Dear Sir, Approximately distance will be around 15 to 20 meters. waiting for reply. Thanks Shoaib |
11/9/2016 1:54 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
Hello, yes then you can use the CP5711 and connect it to the CPU315-DP.
Christoph |
11/10/2016 11:52 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
Hello, WinCC Runtime is enough.
Christoph |
Follow us on