1/29/2010 1:27 PM | |
Joined: 10/7/2005 Last visit: 7/25/2024 Posts: 3011 Rating:
|
Hello Roby I'm afraid it can NOT do so without any additional "extras". The 315-2DP/PN has only one physical 9 Pin RS485 port on board which you configure to be either a MPI OR Profibus DP port (it can't be both together though). What you could do though is to configure the onboard port as MPI port and then add a CP342-5 card to the PLC which will give you a Profibus port (DP Master or DP Slave or FDL comms related). I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on