Industry Online Support
Technical Forum
6/8/2012 3:42 PM | |
Posts: 7 Rating: (0) |
Dear All: I would like to seek your help in checking if there are any mistakes in the configuration I have attached herewith. I will be using CPU 315 PN/DP as a client to get info from 3 different modbus servers. I used the simulator to verify my configuration first before proceeding to the site to install the program. I am a new user of the modbus TCP and i used the sample included in CD we purchased. Basically I just need to read data from the 3 modbus servers starting at holding register 40100 to 40124. I hope you can help me verify and correct my program before I proceed to the site. Thank you so much RodelV
Attachment060812_1.zip (338 Downloads) |
6/15/2012 5:47 PM | |
Posts: 7 Rating: (0) |
By the way this is the program that I used.I hope you can give me an idea on what is wrong with my configuration. I only need to read holding register 40100 to 40125 for 3 three different machines using 10.0.0.1 to 10.0.0.3 ip add for the three machines. Thanks.. RodelV
Attachment061512_3.zip (342 Downloads) |
6/18/2012 10:05 AM | |
Posts: 7 Rating: (0) |
Dear Sakura Thanks for the reply, I will record the net traffic and post here.
|
Follow us on