9/9/2009 9:04 AM | |
Posts: 133 Rating:
|
Ok i tried but screenshot file is too big; siwarex is 7MH45531AA41
|
9/9/2009 2:10 PM | |
Joined: 1/4/2007 Last visit: 9/2/2024 Posts: 1142 Rating:
|
Hello automation_1, On the configuration package CD of the Siwarex M module, there exist a "setup.exe"-file to integrate the Siwarex M module into the HW Catalogue. But if you don’t want to change the HW Configuration, it is not necessary to install that software. Into your Step7-program, there exist a function (original: FC41, but maybe the number was changed in your case.). This function is called “FC_SIWA_M” and handle the communication between the Step7-program and the Siwarex M module. This function has the two parameters “INST” and “IND” (see also the attached file). The parameter “INST” represent a DB-number. Into that DB, you can find the weight value at the address DBD320 (format: DINT). Best regards Siwarexi AttachmentFC41.pdf (317 Downloads) |
Follow us on