12/2/2018 10:21 AM | |
Posts: 8 Rating: (0) |
Hey guys, I have an upload of an HW config from a client with multiple stations via profinet and profibus. For the majority of the HW I managed to find GSD's but there are several stations that I require your assistance: 1. 8DR.GSD Mkv Gateway. 2. gsd.v.2.gsd profi232, the next link is for the GSD download but it requires from me user and password that I don't have http://www.diniargeo.com/prd/scales/weight-indicators/communication-interfaces-en/en-profibus.aspx 3. et200sp profinet- gsdml-v2.33-siemens-et200sp-20171124.xml I attached the project. Thank you in advanced!!!! AttachmentCpu_main.zip (101 Downloads) |
Last edited by: AutoGen_330375 at: 12/2/2018 10:22:48 AM |
|
Follow us on