Industry Online Support
Technical Forum
10/9/2006 3:42 AM | |
Posts: 1 Rating: (0) |
I use PN port of CPU 317-2PN/DP for Ethernet. Can I use this port to communication Modbus TCP_IP ? |
10/9/2006 8:40 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Dear hung_toc_bac, Siemens has got a solution for Modbus/TCP in SIMATIC, this is form IT4Industry. In the following link there is some more information about this: SIMATIC CP protocol enhancements - Modbus/TCP But the information is only talking about the combination with CP-cards so this is not possible wit a PN-CPU. [:(] |
Best regards, |
|
Follow us on