3/30/2020 12:32 AM | |
Joined: 10/7/2005 Last visit: 7/15/2024 Posts: 3009 Rating:
|
Hi Varadharajan.S not enough information to help I'm afraid and the question remains what error value you get in the STATUS word of the Modbus Blocks? Note that the outputs values of these Blocks are only valid for one scan so add capture logic to your program to grab the STATUS value if the error bit is true and the use the manual to see what is going on. |
Cheers |
|
Follow us on