10/5/2022 6:11 PM | |
Joined: 3/14/2008 Last visit: 5/31/2024 Posts: 2070 Rating: (928)
|
Hi SeSa_eng, Unfortunately, you are bound to the hardware limits of the CPU410E. The CPU410E can only handle up to 200 PO meaning you must replace the CPU410E with CPU410-5H. The 410-5H is a scalable CPU. This means you have the best hardware specifications, and you scale the CPU according to your needs by buying PO. PO is available in range 100 to 2600. The PO are stored on a SEC card (small card inserted in the back of the CPU) and you can upgrade it to your needs. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on