6/21/2010 12:15 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello, 1. Check the Diagnostic buffer of CPU. 2. Automation System S7-400 CPU Specifications Best regards, Hristo Mihalev |
6/21/2010 1:06 PM | |
Joined: 5/28/2008 Last visit: 8/4/2024 Posts: 4515 Rating:
|
Hello Vinny, In addition to Umencho's post. Please find here these useful FAQs Using the diagnostics buffer of the SIMATIC S7-CPU Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? |
Ayman Elotaify |
|
6/21/2010 1:47 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
There have restrictions on GD packages in S7-300. Check again your settings according Options for communications via MPI |
6/21/2010 8:05 PM | |
Joined: 5/28/2008 Last visit: 8/4/2024 Posts: 4515 Rating:
|
Hello Vinny, Did you checked that for data you want to transfer from S7-300 to S7-400 that you have set the S7-300 as sender? Please see the second post of this thread Hope this helps |
Ayman Elotaify |
|
Follow us on