10/22/2009 8:39 AM | |
Joined: 5/4/2009 Last visit: 11/23/2024 Posts: 914 Rating:
|
Dear experts... I am facing a problem in the SIMATIC configuration, and the problem is: I have CPU414-2DP & TP27, and the touch panel shows me the following message:" 44 Transfer error #8". And sometimes some LEDs on the PLC are on (CRST + STOP + INTERNAL FAULT) during start up (but recently this problem is solved, because I have changed the memory card). If any body can help me I will be greatfull. I do appreciate your support. Tomy the Master. |
Aim Higher |
|
10/22/2009 11:43 AM | |
Posts: 47 Rating:
|
http://www2.sea.siemens.com/NR/rdonlyres/4E138DCF-C48F-4CE2-B0B8-154A4D34A608/0/out.html |
Follow us on