12/10/2020 12:27 PM | |
Joined: 2/16/2016 Last visit: 1/8/2025 Posts: 7 Rating: (0) |
Hi thank you... I read 93 % in online diagnostic and 67% in the call structure list. |
12/10/2020 1:26 PM | |
Joined: 7/9/2015 Last visit: 1/15/2025 Posts: 4102 Rating: (617)
|
Hi, the value under Online & Diagnostics is different to i.e. the Information you get under Program info. On Program info you get less bytes because it contains only Code block but not Hardware configuration or connection configuration. So it´s different. Please check the following FAQ: How do you estimate the memory requirements of your project in the load memory of a SIMATIC S7-1200/S7-1500?and this: When downloading to the S7-1500 CPU, why is the message "There is insufficient memory on the memory card for this amount of data" displayed although there is still enough memory available?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
Follow us on