4/2/2012 10:22 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello KG*, Can post your code related to the LED status, or Tell me which Function block you have used to Read the Status of the CPU ? OR Here is the Code & Document for the How do you read out the operating state and status of an H system? so replace your code with above one |
Ammy |
|
4/2/2012 1:49 PM | |
Posts: 13 Rating: (0) |
Dear Ammy, The CPU is the same in both the hardware configurations, CPU 414-4H. Logic is written for the CPU's on Rack 0 and Rack 1. Please see the attached backup for the CPU LED status. Thanking in advance... AttachmentCPU_Status.zip (404 Downloads) |
6/23/2014 12:37 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intoWhat is IFM1F in the Led status. With best regards, Narrator1
|
Follow us on