5/18/2016 3:18 PM | |
Posts: 2 Rating: (0) |
Hi everybody. I want to ask one thing. Can i use a 214-1BD23-0XB8 instead of a 214-1BD23-0XB0. What is the difference between them? Than you for your interesting. |
5/18/2016 4:20 PM | |
Joined: 9/27/2006 Last visit: 10/9/2024 Posts: 12285 Rating: (2685) |
Hello static-x; These links are the result of a search for the part numbers mentioned on the Product Support pages (usingnthe search box at the right of this page): ·Product links 6ES7214-1BD23-0XB8 CPU 224-CN, AC PS, 14DI DC/10DO RELAY 6ES7214-1BD23-0XB0 CPU 224, AC PS, 14DI DC/10DO RELAY The difference between the 2 models is the -CN extension in the product description. A few years ago, Siemens developed a "lower-cost" S7-200 (and some HMI panels) line exclusively for the Chinese market, designated -CN. Note that also there is no UL certification for the -CN CPUs, only CE (Appendix H of the S7-200 System manual describes the certifications - very briefly... see attachment). See for example the following discussion on the same subject (there are quite a few more on the forum pages): S7-200 CN https://support.industry.siemens.com/tf/ww/en/posts/71606/ Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/19/2016 1:25:28 PM |
|
This contribution was helpful to2 thankful Users |
5/20/2016 2:49 PM | |
Posts: 2 Rating: (0) |
Thank you so much for your helping to me dchartier. |
Follow us on