11/6/2020 11:08 AM | |
Joined: 2/1/2020 Last visit: 4/4/2024 Posts: 2 Rating: (0) |
Hi All, I am facing a reboot problem with CPU 410 SMART, In diagnostic buffer, it is showing CPU REBOOT to eliminate data inconsistency. then it executes the memory reset, We have EPROM so that the program gets loaded from EPROM. After Restart all DBs got reinitialised. Both the Redundant CPUs warm restart happening, this problem is Occurring frequently. I tried the entire compilation of the program and done the entire download of the program. I have attached the diagnostic below. How to eliminate this problem? Kindly post your suggestions Thanks In Advance S7-410 SMART 6ES7 410-5HN08-0AB0 Firmware V 8.2.0 Boot Loader Firmware expansion V 8.1.0
AttachmentDiagnose_2.txt (293 Downloads) |
11/19/2020 11:14 AM | |
Joined: 2/1/2020 Last visit: 4/4/2024 Posts: 2 Rating: (0) |
Thanks for your suggestions |
Follow us on