11/20/2014 5:41 AM | |
Joined: 11/9/2008 Last visit: 12/21/2024 Posts: 410 Rating: (6) |
Dear All, I have S7300 CPU 315 T ( 6ES7315-6TH13-0AB0) is running on site. We need spare CPU for the same so we got successor product for sameCPU (6ES7315-7TJ10-0AB0). I want know whether I need to download all program or just need place old MMC card in new CPU?? please let me know what is proceduer for the same. I don't want to downlaod program in new CPU because lot of parameter is set or initialize. Please let me which is best procedure for same. Regards, Yogendra. |
11/20/2014 7:34 AM | |
Joined: 4/22/2010 Last visit: 1/15/2025 Posts: 5697 Rating: (715)
|
Hello, More information you find here: Sales and Delivery Release for Innovated Technology CPUs Even if the mmc can be replaced in the new CPU ,I would still backup the old CPU or at least the machine parameters. Regards, Marcjan |
Problem solved? |
|
11/24/2014 3:09 PM | |
Joined: 10/5/2006 Last visit: 1/28/2025 Posts: 74 Rating: (3) |
Hi YogendraG, The best practice for replacing an older S7 CPU with a newer one, is to completely backup the MMC first, without removing the MMC from the CPU! My method is to create a new project and use the "Upload Station to PG" in SIMATIC Manager. If the CPU is defective and not accessible, then you need to read out the memory card using a Siemens USB Prommer (external MMC reader). Unfortunately, there ispossible loss of current values if the MMC is removed from the CPU, but if you have no choice but to remove it... you will have to re-enter them. In principle, if Siemens declares a CPU to be "Spare Part Compatible", it means youshould simply be able to take the MMC out of the older CPU and place it into the new CPU with no changes to STEP 7 required. I've found from experiencethat after uploading from the old CPU, I usually had to download only my data blocks (DB's) (from thenewly uploaded backup project!)back to the new CPU to retain my "online" vaules. The linkbelowdeclares the newer CPU to be"Spare Part Compatible" for your older CPU: http://support.automation.siemens.com/WW/view/en/74785839 I hope this helps. Shawn |
Automation Programmer |
|
11/25/2014 5:43 AM | |
Joined: 11/9/2008 Last visit: 12/21/2024 Posts: 410 Rating: (6) |
HiShawn. Thanks your help. I will try what you mention above. Regards, Yogendra G |
Follow us on