Industry Online Support
Technical Forum
2/14/2010 1:07 PM | |
Joined: 10/7/2005 Last visit: 7/25/2024 Posts: 3011 Rating:
|
Hello egy_eng sounds strange and I can currently only speculate based on the info you supplied. While there were a number of revisions for your 944 CPU, I am unable to find any pointers for your problem in them (you can find a fair few revision release notes Updates HERE). It is conceivable thatyour program worked "correctly" (or in a certain desired way) in an older revision CPU because it "exploited" one of the bugs or undocumented features in that revision. If the later revision fixes the bug, you programwould then behave differently. A somewhat more likely explanation is that theS5 program that you downloadedis notfully the same as the one that was running in the older revision CPU (e.g. general out of date backup and/or DB contents out of date with for example outdatedSetpoints or tuning parameters). My question to you is: Can you switch back to the old revision CPU andverify/repeat the difference in behaviour by using exactly the same S5 program? It would also help to post your S5 program here and tell us about the block or part of the program that "misbehaves" and how it "misbehaves". That's all I can think of for now and I hope it helps |
Cheers |
|
Follow us on