2/18/2010 12:03 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Hello, I must select a new cpu in order to use 7.1. Parts of the old plc-> power supply, rack can be re-used and also we can get a new cpu 416. Now i'm little confused aboutthe PCS7 bundle cpu's. Now I would like to know if there is a difference in usingseperate products (powersupply, cp443-1, cpu, rack etc.) instead of the pcs7 bundles. Because the pcs7 bundles are already preassembled and configuredwith a license... We don't necesarily need them? |
If I could help you, you can use the RATE button. Thank you. |
|
2/18/2010 1:10 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
yeah I thought so, Also, the pcs7 bundles are not available at our standard supplier... only at siemens pcs7 partners or siemens itself.. so that also confused me Thx for the quick reply Regards.... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on