8/15/2020 7:38 AM | |
Joined: 9/3/2008 Last visit: 11/14/2024 Posts: 928 Rating: (163) |
Hi, Since there is no obvious clues about the reason, then I would suggest to upgrade the cpu with the newest firmware. You mention it is currently v1.7. The newest firmware for your model is 1.8.5. It can be downloaded at: Firmware Update for CPU 1516-3 PN/DP After upgrading the firmware, you do not absolutely need to change the firmware version in the project, but I do recommend it. |
Michael |
|
This contribution was helpful to1 thankful Users |
Follow us on