4/29/2010 12:43 AM | |
Joined: 2/23/2007 Last visit: 2/19/2023 Posts: 75 Rating: (1) |
Hi everybody, The load memory using 80%. My problem is in the Work memory (100%), because of this i cannot make online changes or download a individual blocks in my cpu. The system order to compress memory. It says that compress is complete, but it is still 100% assigned. As you understand, i try to download an FC and it says "unable to copy FC". Anybody have any idea how I can expand this memory. I already try to use a Memory flash,but still I can not change the program online. AttachmentMemory RAM.pdf (377 Downloads) |
Follow us on