4/7/2006 10:18 AM | |
Posts: 5822 Rating:
|
Hi tremendo, as you mentioned you have CP 343-1 Lean. So I guess you have ISO on TCP Connections configured, because they would be the best in this situation. For ISO on TCP Connections I found on theQuick Start CD from SIMATIC NET the following Sample: Best Regards J_Bell AttachmentTCP IP Sample S7-300.zip (936 Downloads) |
Last edited by: J_Bell at: 4/7/2006 10:20 AM |
|
5/14/2006 5:37 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi, I believe you can't communicate between this equipment. [:(] A S7-300 is a Server and the CP343-1 Lean is also a Server. [;)] You need on one place a S7-400 or a CP343-1 (bigger then the CP343-1 Lean), it is also possible to take a CPU315-2PN, that one could also be a client. [:P] See also the next link on the Automation & Drives support pages: http://support.automation.siemens.com/WW/view/en/22553424 |
Last edited by: Late at: 5/14/2006 5:38 PMCP341-1 changed in CP343-1 so that it is clear ;-) I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
5/16/2006 9:07 AM | |
Joined: 4/3/2007 Last visit: 4/15/2024 Posts: 35 Rating:
|
[quote user="marcboss"]Hi J_Bell, Could you send me some document to help me about CPU315-2DP and CP343-1 Lean Ethernet Comunication with a PC Station + Ethernet + OPC Server ? Tks, Marcos [quote user="Late"]Hi, I believe you can't communicate between this equipment. ![]() A S7-300 is a Server and the CP343-1 Lean is also a Server. ![]() You need on one place a S7-400 or a CP343-1 (bigger then the CP343-1 Lean), it is also possible to take a CPU315-2PN, that one could also be a client. ![]() See also the next link on the Automation & Drives support pages: http://support.automation.siemens.com/WW/view/en/22553424 Sorry, it's not correct. The CPU and the CP could only work as server, you're right. But in this case the pc station will be the client so that there should be no problem to configurate. Have a look at this FAQ for a step by step introduction: http://support.automation.siemens.com/WW/view/en/15355168 If you use SIMATIC NET cd edition 2005 please have a look at attachment. You'll find this manual also in your start menu under simatic - simatic net - configuration console. AttachmentOPC_S7_IE_englisch.zip (610 Downloads) |
Last edited by: Jörg at: 5/16/2006 9:10 AM |
|
Follow us on