5/27/2011 12:25 PM | |
Posts: 50 Rating:
|
HI Thanks for the reply i have CPU412-3H with CP443-1 at one side other side CPU314 withCP343-1Lean |
5/27/2011 12:49 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, Check there https://www.automation.siemens.com/net-static/Quickstart2009/quickstart012003/html_76/ethernet/ie_tcp.htm Best regards, Hristo Mihalev |
5/27/2011 1:22 PM | |
Posts: 691 Rating:
|
You can configure simple S7 Connection to both CPU and use either AG_Send/AG_Recieve or Get/Put Function |
5/27/2011 1:33 PM | |
Joined: 1/28/2009 Last visit: 6/11/2024 Posts: 6841 Rating:
|
Hi Check here for variety oof sample configurations and programming tips.But, those examples needs basic knowledge about the communication functions used in them. regards Industrial Ethernet - TCP/IP Protocol with S7 Communication between two SIMATIC S7 Stations |
5/28/2011 10:05 AM | |
Posts: 50 Rating:
|
Hi S7 connection is not able to configure in cp343-1lean with cp443-1 |
5/28/2011 11:37 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Not in CP343-1 lean, you should configure the connection in Cp443-1 sides, as already it was mentioned above from Shar best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/28/2011 11:38 AMtypo |
|
5/28/2011 12:48 PM | |
Posts: 691 Rating:
|
Yeah you will see the connection on 400 station not in 300 station |