4/14/2011 10:07 AM | |
Joined: 11/25/2009 Last visit: 5/5/2024 Posts: 33 Rating: (0) |
Hi, i initialize the port 0 of my cpu 226 as a slave but when i open modscan which acts as a master the din bit is high and on error bit i recieved 7 which means CRC error can any one help me out regarding this, Attachmentmodscan+s7200.zip (570 Downloads) |
12/18/2016 5:44 PM | |
Posts: 4 Rating: (0) |
Thank you for having interests in my question. Here I uploaded my PJT. During mornitoring, I can see the error code 7 "receive CRC error". - CPU 226 / Configured as Modbus Slave / Baud Rate 19,200 / Data bit 8 / Stop bit 1 / Parity none Best Regards. AttachmentSAND_FILTER_161217_REDUNDUNT(S).zip (505 Downloads) |
Last edited by: SWKO84 at: 12/18/2016 5:46:22 PMLast edited by: SWKO84 at: 12/18/2016 5:49:35 PM |
|
12/19/2016 6:10 AM | |
Posts: 4 Rating: (0) |
Thank you for helping me. That program I've got from my service provider but they didn't reflect the communication with our device (terminal server as master_Manufacturer: Systech) for Honeywell System. Then they disappeard :(...... So I added Mbus Init and also Mbus_Slave module after check the manual..... Anyway I tried to get communication response from CPU 226 using my PC as attachment. I asked to response I0.0 (address : 10001) and also tried to get response Q0.0 (address 00001): With this way in attachment, I've got no.7 error (receive CRC error) in mbus_slave module when my PC poll to cpu 226. Best Regards. AttachmentConfiguration of Communication Test.pdf (527 Downloads) |
1/4/2017 2:05 PM | |
Posts: 3093 Rating: (323) |
Hello, Regards, |
2/14/2017 9:48 AM | |
Joined: 5/28/2014 Last visit: 10/21/2024 Posts: 32 Rating: (0) |
Dear All. I am facing somewhat same problem. i have no errors in the MB blocks. it shows "0" in both blocks. But in MB_Slave block Done bit is not active and when i check it in simulator ModScan32 it is saying "Checksome Error In Response Message" "Modbus Exception Response From Slave Device" i have no idea what i am doing wrong. Can any one help me. AttachmentModbus Slave.zip (497 Downloads) |
Follow us on