8/23/2018 11:33 AM | |
Posts: 3 Rating: (0) |
Hi, My suggestion: LOGO! Web Editor V1.0 |
This contribution was helpful to1 thankful Users |
8/23/2018 5:38 PM | |
Posts: 5 Rating: (0) |
The app seems to be free in Play store. I can't find a mention of pricing. Maybe it's per button you have to buy or something? |
8/23/2018 5:39 PM | |
Posts: 5 Rating: (0) |
And is there any API I could use? |
8/24/2018 6:00 AM | |
Joined: 10/20/2015 Last visit: 5/21/2024 Posts: 94 Rating: (19) |
Hello vince80, You don't have to create an app. You can if you want, but the App from Siemens is an excellent one. You can add a button and much more. Check the attachment. Page 34, "Adding a control button". AttachmentLogo_APP.zip (100 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on