5/2/2009 4:32 AM | |
Posts: 14 Rating:
|
Hi, I have created a simple FB of an on-off valve. Now, I want to insert ALARM_8P block into this FB so that it can give some alarms such as Valve Fault, Fail to Open, Fail to Close... I tried to do this but I couldn't. Can anybody give me some guidelines to implement it, please? Thank you AttachmentS7 Program(1).pdf (209 Downloads) |
5/4/2009 8:32 AM | |||
Joined: 4/5/2006 Last visit: 6/25/2024 Posts: 917 Rating:
|
Hi hyokoon, in add what Nil correctly said, have a look to following link (hope can help a lil)
Regards |
||
5/6/2009 11:23 PM | |
Posts: 2661 Rating:
|
Hi hyokoon, Which version of PCS7 are you using? I remember in older versions there were problems when trying to insert messages in block types... Regards |
5/9/2009 2:46 PM | |
Posts: 14 Rating:
|
Hi Phantom75, Mine is version 6.1, is there any proplem with this version and how to overcome without upgrade to the newer one. |
6/5/2009 10:27 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi hyokoon The Alarm_8P block can you only use on 400 PLCs. Which hardware do you use/programming for? regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
8/4/2009 11:27 AM | |
Posts: 34 Rating:
|
hi khairul when u call alarm_8p block, u will notice there is a event id which will be automatically generated For to work in Subroutine FB, Alarm_8p has to be in static of the Valve FB STEP A) U have to create Dword of name "MSG_EVID"in IN of the Valve FB, with attributes S7_a_type =alarm_8p S7_server =alarm_archiv ThisMSG_EVID has to be linked to EV_ID of the Alarm_8p block U can call this Valve FB in static of common FB for example if u call this 5 times in the static, u have to create 5 parameters in the IN like STEP A when u call this block in OB1, u have to assign DB, once u assign DB the event id will be automatically generated Attached is the sample program i hope it will work regards dilipan AttachmentAlarm.zip (206 Downloads) |
Last edited by: dilipan_c at: 8/5/2009 3:09 AM |
|
Follow us on