12/10/2016 3:43 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi yasinEncoder, You can do this the following way: 1. Go to your multiproject in Component View and right click 2. Go to Multiproject->Create into multiproject. 3. Go to tab: "Libraries", give it a name and make sure you select the correct path where you want to store the library, make sure this is in the multiproject, so that during archiving, the library is saved as well. The library is now created. I suggest you will set the library as Master. This is recommended for PCS7 projects. You can archive the master library and distribute it to other projects. Also, blocks in the master library are not updated when a new PCS7 version is installed. It is also the place to adjust blocks like adjusting attributes for specific blocks. Normally, I use a project library, not master if I want to create project specific functions. You can create the master library as follows: 1. Right click on the created project library 2. Select Multiproject->Define as Master Data Library You will see the color change from green to blue. It does not change anything, but it is indicated that you have a master library set. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
3 thankful Users |
12/12/2016 8:03 AM | |
Posts: 57 Rating:
|
|
Follow us on