Industry Online Support
Technical Forum
3/14/2007 1:29 PM | |
Posts: 4 Rating:
|
Hello, We have the system with one ES, a redundant server (SRV1 & SRV2), and oneClient system. In ES project i genaratethe server data whit the os compile. After that, i have assign server for the OS. Than i download the project to the srver1 stby server and client. Than i must see on the client ower the server online. Wenn i look to the server data on the client project, i see the serverdata file but the info path for packeages is from ES PC ( \\es\project\es\srv1\packages\xxx.pck). but always is the same. Normaly must be see to SRV1 pc for the packeges. What can the problem? |
3/14/2007 1:36 PM | |
Joined: 9/13/2005 Last visit: 11/18/2019 Posts: 86 Rating:
|
Hi, what you see is the correct behaviour. Package is loaded from SRV1 folder from the ES. Or do you have problems with the automatic package update? The package on the client should have the same timestamp as on the SRV1 |
Best Regards - Mit freundlichem Gruß - yoroshiku onegaisimasu - Sincères salutations |
|
3/15/2007 9:58 AM | |
Joined: 9/13/2005 Last visit: 11/18/2019 Posts: 86 Rating:
|
Hi! Timestamp means the date when the Package file was created. Check the date in WinCC Explorer->Serverdata Regarding the connection problems between server and client. Please check following FAQs: http://support.automation.siemens.com/WW/view/en/18967416 http://support.automation.siemens.com/WW/view/en/22592354 |
Best Regards - Mit freundlichem Gruß - yoroshiku onegaisimasu - Sincères salutations |
|
Follow us on