2/21/2013 5:18 PM | |
Joined: 3/14/2008 Last visit: 12/21/2024 Posts: 2156 Rating: (968) |
You can use: Compile as block type: 1. Create CFC 2. Put motorblock in it, along with driver blocks and your logic for feedback 3. Compile as block type (In chart, goto Chart in the header and select the "Compile as block type" function. 4. Edit all necessary parameters (which one you need to show in WinCC and others) 5. Create block type. 6. Insert from Blocks folder the newly created block type |
If I could help you, you can use the RATE button. Thank you. |
|
2/26/2013 5:02 AM | |
Posts: 45 Rating: (1) |
Thank you Oreca, Could you give any link(document) for creating this type of chart, it will be help full for me. Thanks and regards, Doggalli. |
2/26/2013 8:19 AM | |
Joined: 3/14/2008 Last visit: 12/21/2024 Posts: 2156 Rating: (968) |
Hey doggalli, Here you can find the document...section 10.4 http://support.automation.siemens.com/WW/view/en/60283984 This document is for 8.0, but is same for 7.1 and maybe previous versions |
Last edited by: Oreca at: 2/26/2013 8:28 AMLast edited by: Oreca at: 2/26/2013 8:26 AMIf I could help you, you can use the RATE button. Thank you. |
|
2/27/2013 11:05 AM | |
Posts: 45 Rating: (1) |
Thank you Oreca. |
Follow us on