12/1/2017 7:38 PM | |
Joined: 1/23/2013 Last visit: 8/10/2022 Posts: 226 Rating: (5) |
the days off they do not work .... maybe someone can help in the program ... CTRL_HSC_EXT =does not work does not count pulses CTRL_HSC =OK Attachmenttemp_hsc_1_20171201===.zip (559 Downloads) |
Last edited by: SAR-CNT at: 12/1/2017 7:41:17 PM |
|
12/1/2017 10:38 PM | |
Posts: 103 Rating: (37) |
The description in the system manual is a bit thin but seems good enough. The English descriptions of the HSC_Count structure is attached. AttachmentHSC_Count structure.zip (716 Downloads) |
12/2/2017 2:24 PM | |
Posts: 2826 Rating: (686) |
Hello.
Yes that is a dreadful situation. As "luck" would have it, I am in the process of transitioning from TIA13 to TIA14. I am spending some time to see what changes are available in TIA V14 SP1 Update 3. Earlier this week I was researching the HSC . Studying the System Manual I found some helpful tips. What you ask is attached as a PDF.. an extract from the manual. There are more information there too. I will only be testing my efforts for a project later the coming week. Any hints you could provide when you test yours, will be most welcome. Regards. Update: Attachmentfiles.zip (507 Downloads) |
Last edited by: #dP at: 12/2/2017 2:30:52 PMLast edited by: Jen_Moderator at: 12/4/2017 7:36:14 AMAdded picture and pdf as an attachment. |
|
This contribution was helpful to1 thankful Users |
Follow us on