3/8/2016 9:23 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, Message 13000: The difference between the CF are that the old have a performance licence and the new one not, so this is the reason for the Message 13000. This was wroten in my first post! You have another CF Card without any performance option but for the project it looks that you need the performance option! So you can try to buy a performance Option for you new CF Card and enter the licence to activate it, then this message desapear.
Christoph |
Last edited by: ChristophD at: 3/8/2016 9:24:30 AM |
|
This contribution was helpful to1 thankful Users |
3/8/2016 10:21 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, a CF Card can be ordered with or without the Performance Option. For FW V2.6 from the functionmanual Information regarding the Performance 1 option
computation time utilization greater than 50%. The remaining computation time is displayed in parameter r9976[2]. As of a CPU runtime utilization greater than 50%, alarm A13000 is output and the READY LED on the Control Unit flashes green/red at 0.5 Hz. Regards |
3/8/2016 11:05 AM | |
Joined: 8/25/2014 Last visit: 7/2/2024 Posts: 166 Rating: (2) |
Dear Expert, last thing, what is exactly the performance option means? |
3/8/2016 11:24 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, i don't understand the question! regards Christoph |
Follow us on