2/1/2013 4:24 PM | |
Joined: 10/11/2006 Last visit: 6/5/2024 Posts: 5857 Rating: (793)
|
Dear Mr./Ms Mnada |
With best regards, |
|
2/1/2013 4:29 PM | |
Joined: 10/11/2006 Last visit: 6/5/2024 Posts: 5857 Rating: (793)
|
Sorry, here the attachment. AttachmentD:\temp\E-2.pdf (128 Downloads) |
With best regards, |
|
2/1/2013 6:27 PM | |
Posts: 76 Rating: (0) |
ok. thank you very much was the manual I was looking to do my job. very good
|
This contribution was helpful to1 thankful Users |
2/13/2013 11:37 PM | |
Posts: 76 Rating: (0) |
hello dear I turn back to your aid. After several adjustments move the team to achieve online but that was set parameter in 1070 = r2050 1070 = 0 and guess who walked with ai0 as secondary setpoint p1075. After I could not do more walking. Tells me not ready. You should have an offset somewhere potentiometer makes rocker and would move to one side or the other, but I see no where ..... Attached file if you can see something I do not see. Please review the p2080 you change the values to go there I enter probando.y enabled but the rate of change of speed is very little AI0 analog potentiometer. should be the main setpoint control word? Apparently two words should receive and send 2 but when I change the p2022 = 4 words and move control word 1 is around 00 trillion zero. Good opinions are welcome Thanks in advance
AttachmentTest_sin_consigna.zip (103 Downloads) |
Follow us on