12/5/2019 10:56 AM | |
Posts: 6 Rating: (0) |
Hi i have cu240E 2 DP . i need to set 2 limit switches for stop motor .First need to stop motor in positive direction a second one for stop in negative direction . when i reach positive limit switch need to stop motor and thru communication set him opposite way to move. don't want to move immediately in opposite direction .I upgraded firmware to 4.7.10 and using Starter 5.3.03 .I find this manual https://support.industry.siemens.com/cs/mdm/109757230?c=101839462923&lc=en-WW and don't working as i want .I'm using DI1 and DI2 for limit switches .If someone can help me with correct configuration . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/05/2019 14:03:40New subject after splitting |
|
12/19/2019 7:59 AM | |
Posts: 6 Rating: (0) |
Really thanks for help |
Follow us on