4/25/2016 6:02 AM | |
Joined: 2/9/2013 Last visit: 1/6/2024 Posts: 11 Rating:
|
Hello All, I Have CU250S-PN which is controlled by S7-1200 over Profinet. i have small positioning application of Rotating table. my encoder is TTL with 1024 pulses which i am going to connect to Drive. so my query is, i want to read encoder in PLC, because it is TTL (5VDC) i can not read it directly, so is it possible to read encoder Counts on Profinet? if yes kindly provide the details or sample program. Thanks in Advance.
|
Last edited by: vishal_panchal at: 4/26/2016 7:16:43 AM |
|
4/25/2016 6:45 AM | |
Joined: 11/21/2007 Last visit: 3/11/2025 Posts: 2326 Rating:
|
Hello Yes. You can read the Encoder position over PROFINET. SINAMICS G120: Activating the basic positioner (EPOS) and position control for CU250S-2 FW4.6 in StartDrive V13 |
Last edited by: Navnag at: 4/25/2016 6:48:47 AMThere is no such thing as the last bug in a program |
|
4/25/2016 7:59 AM | |
Joined: 2/9/2013 Last visit: 1/6/2024 Posts: 11 Rating:
|
Thanks for the Response actually the problem is where i want to apply this application, S7 1200 is already there so they don't want to buy license for positioning for this simple job which can handled by 1200. |
4/25/2016 9:20 AM | |
Joined: 11/21/2007 Last visit: 3/11/2025 Posts: 2326 Rating:
|
G120 CU250s - Basic Positioner is Free ... you don't need to buy a license |
Last edited by: Navnag at: 4/25/2016 12:14:19 PMThere is no such thing as the last bug in a program |
|
4/25/2016 10:44 AM | |
Joined: 2/9/2013 Last visit: 1/6/2024 Posts: 11 Rating:
|
it requires license in Drive, Have look Attached.. |
This contribution was helpful to
1 thankful Users |
Follow us on