1/23/2015 5:44 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980)
|
Hi, sorry for this but have you not reade the delivery notes for scout tia? SCOUT TIA V4.4 HF2 configures the SIMOTION C240/C240 PN motion controller as well as the SIMOTION D410-2 and D4x5-2 Control Units, including CX32-2/CBE30-2, in the TIA Portal with kernel/firmware version V4.3 and V4.4. Also, the so-called SIMOTION Drives in TIA Portal. These are SINAMICS S120 drives with firmware version V4.5 and V4.7 provided they are interconnected with a SIMOTION-CPU via PROFINET or PROFIBUS. |
Last edited by: ChristophD at: 1/23/2015 5:46 PM |
|
1/23/2015 5:57 PM | |
Joined: 1/4/2013 Last visit: 4/23/2024 Posts: 1107 Rating: (101) |
Hi Cristoph, in that delivery note they say that it supports S120 but they doesn't say "we ONLY support S120". They could have done a clear list of what is supported and what isn't (like for example for the windows XP/7 compatibility, that is really perfect). Anyway, do you know when the cu305 will be supported by TIA ? Isn't any other way (GSDXML) for using it under TIA ? |
Searching for Siemens used/new equipments ? |
|
1/23/2015 6:26 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980)
|
Hi, thanks i hope it works in your case. if not you can ask anything to solve you problems here. Regards Christoph |
Follow us on