11/8/2017 5:55 AM | |
Joined: 8/4/2014 Last visit: 1/29/2024 Posts: 23 Rating: (1) |
Dears, could you please help me to configure next drive system: - CU type: CU320-2DP FW4.7 - Drive type: Sinamics S120 6SL3120-1TE21-8AA4 - Motor type: 1PH8107-1DD13-2BA1 , YF: J7637 3876 01 002 - Encoder with D-cliq interface: IC22DQ-B35, HEIDENHAIN ERN 1387.035-2048 Problem that I have is with encoder configuration. I have set in drive configurator wizard at encoder configuration window: "Encoder with DRIVE-CLiQ interface" with encoder identification 10000. After that in topology I can see drive object (6) as encoder connected to motor module port 2 After download there are some alarms and online topology does not see encoder. From FCDS (http://workplace.automation.siemens.com/fcdsweb/serv/) I have downloaded 2 bin files and instructions how to set encoder but I didn't have opportunity to try it up to now. Could you please check attachments and just confirm that solution of problem is to follow instructions from FCDS or I need to do something else. Thank you!
AttachmentFILES.zip (141 Downloads) |
Follow us on