2/19/2018 3:36 AM | |
Posts: 137 Rating:
|
Hi, I am going to setup on CU320-2PN I have a some problem When I was diagnostic online, The CU320-2PN Firmware version is V4.50.30 But TIA Portal Firmware version is 4.8 or 5.1 It is different Refer attachment Plz, Let me know how to match Thanks |
2/19/2018 6:11 AM | |
Joined: 5/12/2006 Last visit: 3/23/2025 Posts: 22596 Rating:
|
Hello, update the Firmware on the CF on the CU320-2 PN. https://support.industry.siemens.com/cs/ww/en/view/109740193 https://support.industry.siemens.com/cs/ww/en/view/109751474 Regards |
This contribution was helpful to
1 thankful Users |
2/19/2018 9:31 AM | |
Posts: 137 Rating:
|
Hi, It must be updated via Hardware CF card? Right? Thanks |
2/19/2018 9:39 AM | |
Joined: 5/12/2006 Last visit: 3/23/2025 Posts: 22596 Rating:
|
Hello, yes, delete the old FW on the CF and extract the new one to the root of the CF. Or you use the Webserver on the CU to update the FW if this is possible.
Christoph |
Last edited by: ChristophD at: 2/19/2018 9:41:41 AM |
|
2/19/2018 9:56 AM | |
Posts: 137 Rating:
|
Hi, I have no CF card reader If then, What is the other method? For example, 1st. Is it installable Frimware 4.5 for the Startdrive? 2nd. configurate with STARTER for Firmware 4.5 and then, use it with TIA Portal if it is possible, How to import on the project? 3rd anything else Thanks |
2/19/2018 10:11 AM | |
Joined: 5/12/2006 Last visit: 3/23/2025 Posts: 22596 Rating:
|
Hello, no for S120 no FW V4.5 available (no HSP or something like that) so you can only use V4.8 or V5.1 FW Version. the procedure for a FW Update with the integrated Webserver in the CU320-2 is descriped in the Function Manual of sinamics https://support.industry.siemens.com/cs/ww/en/view/109754299 Regards Christoph |
3/8/2020 7:19 PM | |
Joined: 3/7/2020 Last visit: 9/1/2021 Posts: 1 Rating:
|
4.8 записать версию 5.1SP1 и использовать ключ от версии 4.8 |
3/9/2020 6:04 AM | |
Joined: 5/12/2006 Last visit: 3/23/2025 Posts: 22596 Rating:
|
Please use english language! |
We are working on a new user interface with better overview and more relevance.
Follow us on