1/15/2018 10:10 AM | |
Joined: 10/11/2006 Last visit: 3/17/2023 Posts: 5459 Rating:
|
Hello, I think it is not the question of accessing the infeed. I think you have a problem getting online access to your DP Control Units. You need to try to get online either via Profibus or via X127 Ethernet port. I think going online with X127 in front of the CU is easier. Connect it via Ethernet to your PC, set up the correct PG/PC interface in Starter and search for accessible devices. The default address of X127 is 169.254.11.22. If you reached to get online you need to check p864 on your drives. Which kind of setup do you have? Does each CU have their own Infeed or is there only one central infeed for all drives? Or do you have infeeds without DRIVE-CLiQ interface (SLM 5 / 10 kW)? Are you sure you enabled the infeed before enabling the drives? There are too many open questions to give you a proper advise how to solve your issue. We need more information. Here is a getting started, where you find a description on how to get online with your device (see from chapter 5.2 on): https://support.industry.siemens.com/cs/de/en/view/109754314 |
With best regards, |
|
Follow us on