8/23/2011 10:21 AM | |
Posts: 2964 Rating:
|
Hello.... On your Servcie Display you have some thing called Smooth Current actual value...check this tells you the motor utilization. Regards, Prakash |
8/29/2011 3:04 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Servo motor current depends upon lot many factors. However please find attached here with the data sheet of the said motor. From the sheet you can understand the max current applicable at correspondence duty cycle. Hope this will help you. DEEP. AttachmentData sheet 1FK7105.pdf (167 Downloads) |
8/31/2011 9:13 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, I have never seen any servo motor failed because of winding failure due to overload.By Siemens,it is so superbly built & have protection features that it will not burnt because of overloading or temperature increase. It is well protected from drive side with current & torque limits. For temperature rise, motor has inbuilt thermister to sense winding temperature which in turns protects motor from thermal heating. (All this is true provided, proper engineering of motor & drive designe is worked out & implemented. Also entry of coolant or some foreign fluid which in turn may short winding & may cause motor failure. But I am sure that for this manufacturer or designer should not be held resposbile.) Please see the file attached here with for thermal motor protection. DEEP. AttachmentServo motor thermal protection..pdf (188 Downloads) |
8/31/2011 2:47 PM | |
Posts: 25 Rating:
|
Thank you sir |
Follow us on