3/15/2020 11:28 AM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
HelloChemE, What is the Role of FB 3007 and If its a custom made block, why do you have assigned a number like this? my understanding is as follow from your picture, The TimerP block will send a trigger to the external message of MonDiL block. Better you place the MonDiL block OB order at the end. Now it's earlier to your timer block. And, Better not to connect timerP block Out directly at reset Nub of the same block. I think it may freeze your timer. You can use Flipflop with "R_Trig" and timer mode as "Extended pulse" timer Just have a look at my picture. Try to simulate this after connecting your condition Pass signal to the flipflop "set" nub, and mention your time property at "PON" block. Then, Modify at the end as the way to need the output. |
Last edited by: Maruthakasi_S at: 03/15/2020 11:33:15Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
3/16/2020 9:27 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930)
|
Hi, There is a much easier way without using custom blocks or Set/Reset logic. See attachment. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
3/16/2020 4:53 PM | |
Joined: 2/29/2016 Last visit: 3/12/2024 Posts: 100 Rating: (1) |
Hello Oreca, That looks simple! I was looking for something like this. |
3/17/2020 8:21 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930)
|
Hi, nice! Let's do a challenge...who can make it more easy. Well ChemE, you got plenty of solutions. Good luck |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
7/25/2020 9:51 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930)
|
You can do it all with PCS7 |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on