7/5/2016 9:12 AM | |
Joined: 3/14/2008 Last visit: 5/31/2024 Posts: 2070 Rating: (928)
|
Hi, You are getting warm . You need to do the following things on CFC level: 1. Insert MonAnL block in CFC. 2. Double click on the MonAnL block and fill in a number under: "Create block icon". The numbers: "1", "2", "3" and "4" are defined by the system. You can fill in a number like "111". Make sure you enable: "OCM possible". This means that OCM capable parameters are compiled to the OS. 3. Compile + download the AS. You need to do the following things on WinCC: 1. Copy the template like you already did-> @PCS7TypicalsV8.pdl and rename. 2. Create a copy of the existing MonAnL block icon and open the properties of the block and select the following: System. In there, change the Type property @MonAnL/1 to @MonAnL/111. The extension "@MonAnL/" must be maintained. At this moment, you can compile the OS, where the function: "Create/update block icons" is executed. The system will now create the block icon you adjusted and inserts it into the picture of the corresponding plant hierarchy. 3. What you can do next, is to copy the faceplate files of the "MonAnL". This is recommended when you want to change the faceplate, like adding an additional object. In this case, you will copy all original faceplate files (see below) and change the extension: "MonAnL" to a suitable name like: "MonAnL_Custom", so it will be like "@PG_MonAnL_Custom_Standard.pdl". You can now define your custom block icon to look at the new faceplates instead of the original. For this, you have to set the following: 1. Open the properties of the block icon 2. Go to: "System" and change the extension "PCS7 MonAnL Control" under servername to: "PCS7 MonAnL_Custom Control". Faceplate files of the "MonAnL": - @PG_MonAnL.pdl - @PG_MonAnL_Limit.pdl - @PG_MonAnL_Overview.pdl - @PG_MonAnL_Parameter.pdl - @PG_MonAnL_Preview.pdl - @PG_MonAnL_Standard.pdl - @PG_MonAnL_ViewToolbar.pdl At this moment, when you compile the OS again or just run the: "Create/Update block icon" function separately, the block icon will open the new faceplate when you click on it. But there are still a few things that must be taken care of in the faceplate files itself. 1. Open @PG_MonAnL_Custom.pdl and select the object: "@Faceplate". In the object, select the property: "Firstview" and change the name to: "@PG_MonAnL_Custom_Standard.pdl". 2. Select the object: "ToolbarWindow". In the object, select the property: "PictureName" and enter the name: "@PG_MonAnL_Custom_ViewToolbar.pdl". 3. Select the object: "Objcollection". In the object, select the property: "BlockType" and enter the name: "MonAnL_Custom". These steps will make sure that the block icon you created does not open the original faceplate files, but the custom ones. For more information about this subject, you can see the following document: APL Styleguide see page 87, section 6.4.2: Adapting faceplates. In there is a step by step walkthrough and even some other modifications like changing the toolbar window or authorizations. I hope this clarifies the subject for you! |
Last edited by: Oreca at: 7/5/2016 10:55:06 AMLast edited by: Oreca at: 7/5/2016 11:04:15 AMLast edited by: Oreca at: 7/5/2016 11:18:20 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to9 thankful Users |
7/5/2016 10:37 AM | |
Joined: 3/14/2008 Last visit: 5/31/2024 Posts: 2070 Rating: (928)
|
Because I was not done with my answer yet... |
Last edited by: Oreca at: 7/5/2016 11:19:14 AMIf I could help you, you can use the RATE button. Thank you. |
|
7/5/2016 12:20 PM | |
Posts: 39 Rating: (2) |
Thanks to all! Oreca, thank you very much for the complete response
|
7/5/2016 2:23 PM | |
Joined: 3/14/2008 Last visit: 5/31/2024 Posts: 2070 Rating: (928)
|
You're very welcome |
If I could help you, you can use the RATE button. Thank you. |
|