11/7/2018 12:11 PM | |
Joined: 3/14/2008 Last visit: 6/27/2024 Posts: 2075 Rating: (930)
|
Hi William, "1" in the case you describe means the block icon number which you can define in the block properties in CFC. For creating blocks/block icons and faceplates, please take a look at my topic under "APL section". There are several topics listed where the exact procedure is described to create your own blocks/icons and faceplates. If you have any questions, let us know |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
11/8/2018 9:07 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi William Sylvester, in the attachment you can find a short summary who you can create for own blockicons. I hope it will help you with your issue. The two best manuals for creating own block icons are (these are also listed in the link of Oreca):
with regards AttachmentCreate_own_blocks_with_blockicon.docx (107 Downloads) |
This contribution was helpful to1 thankful Users |
11/8/2018 6:38 PM | |
Joined: 10/26/2017 Last visit: 3/8/2024 Posts: 6 Rating: (0) |
Issue is resolved appreciate the help all |
Follow us on