3/21/2011 4:49 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22229 Rating: (2980)
|
Hello, can you test the format for "1R%4.2f" or "1R%3.1f"? Regards Christoph |
3/21/2011 5:46 PM | |
Posts: 26 Rating: (0) |
Yes. With @1R%4.2f@ the message is: "can you test the format for 105.00" With @1R%3.1f@ themessage is: "can you test the format for 105.0" |
3/22/2011 4:20 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22229 Rating: (2980)
|
Hello, which SIMOTION Version (Scout and FW)do you use? Regards Christoph |
3/22/2011 11:30 AM | |
Posts: 26 Rating: (0) |
Scout V4.1.5.6 D4x5 V4.1.5.10 |
3/25/2011 12:24 PM | |
Posts: 26 Rating: (0) |
I guess I will have to limit my diagnostic messages to integer values. [schnippschnapp] new question is splitted to Is it possible to add the diagnostic messages to the file "DGBUFTXT.EDB". Thank you, ms... |
Last edited by: O_Moderator at: 3/28/2011 7:54 AM |
|
Follow us on