7/2/2019 2:08 AM | |
Posts: 14 Rating:
|
General question: Is there any way in SIMOTION to create a kinematic relationship between 2 cartesian virtual axes and 2 real axes, without using the Path Axis technology object? (The reason I don't want to use the Path Axis technology is that the motion of the Cartesian axes is very complicated and comes from a large amount of existing code, and the Path commands are too simple in this case). Specifically, I want something like: RealAxisPosition_1 = VirtualAxisPosition_1 + VirtualAxisPosition_2 RealAxisPosition_2 = VirtualAxisPosition_1 - VirtualAxisPosition_2 (HERE is an example of the basic concept) Any help or insight into this problem would be appreciated. Thank you |
Follow us on