8/5/2021 8:31 AM | |
Joined: 6/26/2008 Last visit: 1/24/2025 Posts: 253 Rating: (29) |
Hi, I guess you know the following application example?! Integrating user-defined controls into WinCC Unified (Custom Web Controls) I tested it in a small demo project and it was very easy to integrate it. With the help of the documentation I was able to create a small own CWC (just an Input- and a Textfield). I guess the point is that you have to be familiar with "web-programming". This is not my case, so I endet after that short example. Greetings, |
Follow us on