1/25/2018 10:38 AM | |
Posts: 40 Rating:
|
i need (cut machine ac servo system ) program manual to help me when i change my cut machine parameters |
1/25/2018 12:53 PM | |
Posts: 40 Rating:
|
my pc connects to the driver with com port and i will send u the image |
1/25/2018 12:54 PM | |
Posts: 40 Rating:
|
this is cu card |
1/25/2018 12:55 PM | |
Posts: 40 Rating:
|
|
1/25/2018 3:47 PM | |
Joined: 10/11/2006 Last visit: 6/24/2024 Posts: 5866 Rating:
|
Hello, this is a Masterdrives with CUMC board, you find the manual here: https://support.industry.siemens.com/cs/ww/en/view/109736627 But this drive was used for motion control in general, so the cut functionality was realized using standard motion control functions of the drive (there was no standard cutting application). This means, if you need special information on the cutting functionality realized, you need to contact the machine manufacturer. |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
1/29/2018 9:00 AM | |
Posts: 40 Rating:
|
i have semovert masterdrive converter its card (6es7090-0xx84-0ad1) has stopped . do i need any new programming Procedure after putting the new one ? thank u |
1/29/2018 1:37 PM | |
Joined: 10/11/2006 Last visit: 6/24/2024 Posts: 5866 Rating:
|
Hello, you need DriveMonitor to load the parameter backup to the drive. If the old CU is still accessible, you can also take a backup from this CU with DriveMonitor. |
With best regards, |
|
Follow us on