2/16/2015 11:15 AM | |
Posts: 26 Rating: (0) |
Hello, i have a problem on CX32-2 caused by the last firmware 4.4.0.4, i think. Two (CX3 and CX4) of the four Cx32-2 they have the RDY led flashing 0.5Hz (commissioning/reset). Everything semms ok: firmware, parameters. I have powered on several time. The project was converted from 4.3.1.9 and with this firmware was ok. Attached one video and some screenshot. AttachmentCx32-2 rdy led.zip (59 Downloads) |
2/16/2015 12:04 PM | |
Posts: 26 Rating: (0) |
CX3 has a drive deactivated, on CX4 all drives are deactivated. |
Last edited by: HjS_100 at: 2/16/2015 12:04:58 PM |
|
2/16/2015 12:16 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3006)
|
Hi, any fault present on the ssystem? Regards |
2/16/2015 12:16 PM | |
Posts: 26 Rating: (0) |
No, machine is running. |
2/17/2015 10:27 AM | |
Posts: 26 Rating: (0) |
Hello, I tested by activating all drives in CX3 and now it works fine. Attached one video. Don't care about CX2, i used one of its drive. Attachmentvideo_2015-02-17_09-40-25.mov (50 Downloads) |
Last edited by: HjS_100 at: 2/19/2015 2:18:06 PMLast edited by: HjS_100 at: 2/27/2015 12:16:36 PM |
|
Follow us on