8/20/2019 3:33 PM | |
Joined: 1/22/2019 Last visit: 2/25/2024 Posts: 9 Rating: (0) |
Use the S7_Simulator,Just fun to compare the ratio of the Plus between 1ms IEC_Timer and 10ms IEC_Timer in the 1ms Cyclic Interrupt OB. It Should be 10 times, but I find that just 2 times. Could you tell me how to analyse this issue? Otherwise, is it normal in the simulator without hardware? AttachmentCyclic Interrupt 2019-08-20 .avi (59 Downloads) |
Follow us on